Part Number: TUSB3410
Hi team:
customer want to use TUSB3410 in a Pad project to implement UART to USB function, can you help to check if this device support USB Host (master)mode and USB slave mode?
when it is use as slave mode, it can be used as system debugging and log trace?
when it is use as Host mode, it can be used as the input from the external Keyboard?