Hi,
I'm designing a camera using isx019 Sony.
Ser is DS90UB935 and Des is DS90UB936.
We are in trouble without mipi output from Des.
mipi output is fixed at 1V.
Please tell me the solution.
input is mipi-csi2 4lane(format : YUV 8 bit)
Frame Rate = 30Hz
Image Size = 1280x 960
Cable is Coax.
DS90UB935 setting
Synchronous mode(Rhigh open/Rlow 10kΩ)
No register setting
DS90UB936 setting
CSI-2 synchronous back channel mode
register 0x33 →0x03
Are there any registers that need to be set?