Part Number: TCA9509
Other Parts Discussed in Thread: DS92LV0422, , PCA9306
Hi,
We have a board design where the TCA9509 is used as a +3.3V to +1.8V I2C translator with the master device on the B side running at +3.3V and four DS92LV0422 slave TI devices connected to the A side. Ack's from the slave devices are not getting translated across the buffer to the master and the bus is hanging. Looking carefully at the data sheet for the TCA9509, I see now that the DS92LV0422 logic low is specified as .36V max and the TCA9509 has a VILC min of less than .15V. I assume this is why the part is not working. The requirement of a .15V logic level seems very restrictive almost to the point of making the TCA9509 unusable in most applications. Does TI engineering have any suggestions (other than designing the TCA9509 part out) for making the application I have work?
Thanks,
Mitch