This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65988: TIDA-01515 100W Support

Part Number: TPS65988

Hello,

It was indicated in a separate thread (http://e2e.ti.com/support/interface/f/138/p/827776/3069363#3069363?jktype=e2e) that care must be taken to ensure that the cells can support a higher power level, however, is there anything fundamentally limiting TIDA-01515 from sourcing and sinking 100W? Assuming there are no concerns with the cells, could the TPS65988 simply be reconfigured to allow for 5A source and sink?

Thanks,

Chris

  • Hi Chris,

    The only limiting factor in TIDA-01515 is the batteries used. The TPS65988 can be reconfigured to support 100W. Keep in mind that a 5A USB-C cable will be needed to support 5A on TPS65988. This is in alignment with the USB-PD specification.

    Thank you,
    Eric