Part Number: DS26C31T
Other Parts Discussed in Thread: ISO3086
Hi, Staff
Data is transmitted between the following ICs by communication between devices.
① DS26C31TM → DS26LV32ATM
② DS26C31TM → ISO3086DW
In the case of ②, only the DS26C31TM is damaged, and communication is not possible.
(Use only 2 and 3 pins connected)
We measured the (2-3pin) resistance value of the damaged DS26C31TM and shorted it between GND.
There is no communication failure (device damage) in the device combination ①.
What can be the reason why the DS26C31TM is damaged due to the connection in ②?
(Is the device connection in ② causing trouble?)
(No ESD protection element is used for the differential signal line)
best regards
cafain