Part Number: MAX3222E
Other Parts Discussed in Thread: MAX3221
Hi ,
Test the output signal of MAX3221 (V+, DIN1, DOUT1) and find the fluctuation, As shown in the figure, please help analyze it.Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Blanche,
This device (and many other RS-232 transceivers) use a charge pump to take the VCC rail and generate the higher-voltage V+/V- rails that are switched onto the "DOUT" pins to transmit high or low levels to the RS-232 line. These charge pumps will have some ripple associated with them, and the ripple frequency and amplitude are dependent on the capacitance values used and the load current. In this case when the DOUT line is high it is switched to V+, and this V+ rail is sourcing some current to the RS-232 line. This causes the voltage to drop as current is pulled from the V+ charge storage capacitor. Once the voltage reached a level that is too low, it is recharged by the charge pump and the voltage increases back to its regulated level.
You can read more about the operation of the charge pump circuitry and what factors influence the ripple waveforms in this blog:
Please let us know if you have any further questions.
Regards,
Max