Part Number: DS92LX1622
Other Parts Discussed in Thread: DS92LX1621
We have a DS92LX1621 -> DS92LX1622 display mode link that works well other than the I2C master at the deserialiser. The SCL frequency is left at the default frequency of 100 kHz. The I2C bit rate changes back and forth between the expected 100 kHz and 600 Hz. 600 Hz is far lower than can be achieved by programming the I2C bus rate register. Throughout this the recovered PCLK remains at 40 MHz and LOCK is high. I believe that the I2C clock is derived from an internal 25 MHz oscillator rather than the recovered clock anyway. On some deserialiser boards the I2C slave device copes with this, on others it doesn't. DO you have any ideas what the problem may be ?