Part Number: TUSB1046A-DCI
Hi Team,
If we are sure that the USB 3.1 option will not be used with the TUSB1046A-DCI, can we leave EQ0/EQ1 and SSEQ0/SSEQ1 pins floating?
Thanks!
Roy Hsu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB1046A-DCI
Hi Team,
If we are sure that the USB 3.1 option will not be used with the TUSB1046A-DCI, can we leave EQ0/EQ1 and SSEQ0/SSEQ1 pins floating?
Thanks!
Roy Hsu
Roy
You can leave them as No Connect. Please note that SSEQ0/A0 is A0 when in I2C mode, so you may need to pull it up or down to set the proper I2C address.
Thanks
David
Hi David,
Got it. We're not using I2C mode so it should be fine.
Thanks!
Roy Hsu