Part Number: MAX202
Other Parts Discussed in Thread: TRS3232E
Can I remove the capacitor C3 (pin2-vcc)?
Can MAX202IDG4 work properly anyway?
Best regards
Daniele
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Daniele,
No, please don't do that. This capacitor is required for operation of the device's charge pump circuit. You can read more about it here:
Regards,
Max
If I put this capacitor I've a noise on the 5v(vcc), this is the voltage referance for ADC then the value converted it's wrong. If I remove the capacitor the noise disappare and the comunication it's ok. Of course the 10V on the rs232 it's not wonderful but enought for the comunication.
The capacitor is 100nF ceramic. If you've a suggestion wil be highly appreciated
Best regards
Daniele
Daniele,
What kind of noise do you observe with the capacitor? What kind of power design in the system? Have you ever checked if the noise correlates with to charging cycle? I was wondering if the transient current change makes the supply unstable.
Regards,
Hao