Part Number: TUSB8041
Other Parts Discussed in Thread: TPS2561
Hi,
I am using TUSB8041 as 5 port USB 3.0. The upstream port is coming from processor. All downstream ports are working fine when I connect pendrive, keyboard, mouse. Even data transfer is happening between processor and slave. But when I connect USB based DVD burner (used to install OS), installation screen is not coming. Even it is taking long time to enter the BIOS screen. TPS2561 is used as a current limiter. The current limit resister used is 37.3k. I changed to 22k, but still the problem didn't solve. The current rating of DVD burner is 1.5A. Schematic is attached for reference. Kind help is requested.
Regards,