This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A-Q1: PCLK Input jitter

Part Number: DS90UB913A-Q1

Hi, Team,

Question regarding for PCLK input jitter spec specified in datasheet as 0.3UI(max).

Is this needed to think the same as Ser output jitter like 1 UI = 1 / ( PCLK_Freq. /2 x 28 )?

Or could be using just 1/PCLK=1UI?

Thanks,

Best regards,

Koh

  • Hello Koh,

    For the PCLK input jitter to 913A, the UI is specified as the UI of the serialized data rate; in this case

    12bLF mode: 1UI = 1/(PCLK*28)

    12bHF mode: 1UI = 1/(PCLK*28*(2/3))

    10bHF mode: 1UI = 1/(PCLK*28*(1/2))

    Best Regards,

    Casey