This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI84: SN65DSI84: configuration issue.

Part Number: SN65DSI84

Hi Sir,

About SN65DSI84, Now  we use this chip to convert the previously given mipi to LVDS to light up the LCD screen;

The test mode can now be used to light up the LDC and output shows the color bar;

However, in the non-test mode, the converted LVDS data signal is abnormal;

Please help to check what configuration should DSI pay attention to when receiving and converting, and what causes the wrong data signal of the following conversion?

Normal LVDS data signal of test image is:

The LVDS data signal converted by DSI is:

Our configuration parameters is: ( Input dsi is 4lanes and output A+B channel)

write=> 0a: 05
write=> 0b: 10
write=> 10: 26
write=> 11: 00
write=> 12: 2d
write=> 18: 6c
write=> 19: 00
write=> 1a: 03
write=> 1b: 00
write=> e0: 00
write=> e1: 00
write=> 20: 80
write=> 21: 07
write=> 24: 38
write=> 25: 04
write=> 28: 20
write=> 29: 00
write=> 2c: 2c
write=> 2d: 00
write=> 30: 05
write=> 31: 00
write=> 38: 58
write=> 3a: 04
write=> 34: 94
write=> 36: 24
write=> 3c: 00

Thanks and with best regards.