Part Number: DS16F95QML
Dear TI Support Team,
currently I am trying to connect the DS16F95QML serial transceiver to the UART I/O of a µC.
My µC I/O pins tolerate a maximum of 3.8 V (VCC1 + 0.5 V , whereas VCC1 = 3.3 V).
It has already been answered in a question that at pin "RO" the maximum voltage "Vol" is 3.6 V (VCC2 - 2*0.7 V , whereas VCC2 = 5 V).
( e2e.ti.com/.../790289 )
Additionally it was said that this maximum voltage depends on the temperature.
Because my application takes place at high fluctuating temperatures, I need to know how the voltage "Vol" will behave between -45° C and +125° C.
Can it happen that the voltage "Vol" exceeds 3.8 V at any time?
Best regards
Patrick