Part Number: HD3SS3220
Hi,
I am working on external interfaces to the SOM module (NXP i.MX8M), I need to make USB 3.0 implementation as simple as possible on the USB C connector (DFP mode, no additional functionality such as charging, audio, etc.). I would like to use the HD3SS3220 chip in GPIO mode plus a simple USb VBUS switch chip (STMPS2171).
The question is: what signal should control the switching of VBUS voltage? If I connect it as shown in the diagram below, power will be available to the receiver constantly.