Other Parts Discussed in Thread: SN74LV4052A-Q1
Hello guys,
One of my customers is considering using TPIC8101 for their new engine systems. They want to implement 6~8 pcs knock sensors for one engine and they want to read these sensors output using one TPIC8101 only.
For that, they will try to insert analog multiplexer like SN74LV4052A-Q1 between each knock sensor and TI8101 sensor input.
They have the follwing questions at this moment. Could you please tell me your comment for each question?
Q1. Can SN74LV4052A-Q1 be used between each knock sensor and TI8101 sensor signal input as a multiplexer? Or one knock sensor output must be connected to input resistor of inverting amp of TPIC8101?
In other words, in case of 6~8 pcs knock sensors using , is 3~4 pcs TPIC8101 needed?
Q2. They will try to use TPIC8101 EVM. Also they want to know what knock sensor is better for the EVM. So could you show me an example of knock sensor part number which can be connect to TPIC8101 EVM?
Your reply would be much appreciated.
Best regards,
Kazuya.