Part Number: TFP410
Hello
In one of my project we need to add HDMI display. We are using MCU with inbuilt LTDC means RGB888 output. So now we want to convert RGB888 to HDMI Output to connect any monitor. Before i design my PCB i have few questions.
1.> Is TFP410 is right choice for this task?
2> is HDMI monitor size and resolution will be depend on output of RGB888 or HDMI will work independently ?
3> Is I2C bus is must to configure TFP410?
4>what is the maximum resolution& frame rate of monitor that we can connect to output of TFP410?
i am working first time on RGB to HDMI so i not have deep knowledge of it.