Part Number: DS90UB941AS-Q1
Hello,
Can 941 communicate with 948 without the DSI input when 941as is configured in dsi reference clock mode? Auto-switch to internal AON clock is set as default, i think it should be ok (947/9 and 92x works, MCU can read the deseri registers through ser without PCLK), but i failed to read 948 registers through 941as.
I can see the 948 I2C address from 941as but i can't read or write it.
To remote read 948 registers, I have to enable 941as pattern generator (internal pclk) or change to internal reference clock mode, could you help explain the differences between 941as and other FPD-Link III devices?
Dongbao