Part Number: TL16C550C
Other Parts Discussed in Thread: TL16C550D
Hi,
I need to replace the PC16550DVX/NOPB component because it is EOL. The TL16C550CIFNR is suggested as replacement. My application use the component at 5V and with a 22.1184MHz quartz. The datasheet reports that the ACE contains a programmable baud generator that takes a clock input in the range between DC and 16MHz (24MHz for the PC16550D) .
Is this limit valid for 5V and 3.3V operation? I found in other non TI alternatives that such limit may depend on the supply voltage: is this the case also for the TI component?
Thanks.