This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UH928Q-Q1: compatibility between UH928 and UB927

Part Number: DS90UH928Q-Q1

Hi team,

I have a question about the compatibility between DS90UH928 and DS90UB927.

1. If you the data is not HDCP contents, then can you send the data over DS90UB927 and DS90UH928 combination?

2. I would like to know the difference between UB924 and UH928, besides HDCP function and maximum pixel clock.

regards,

  • Hello Shinji,

    Thanks for reaching out!

    1. If HDCP is not used, then UB and UH devices are fully compatible. 

    2. The main difference between Ux924 and Ux928 is the maximum supported pixel clock as you mentioned

    Best Regards,

    Casey