Part Number: DS90UB953-Q1
Hello team,
Can we support 6-8W over PoC? Customer is needing to add a heater on the camera, hence needing to support higher power.
We're considering 953 and 960 for the design.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1
Hello team,
Can we support 6-8W over PoC? Customer is needing to add a heater on the camera, hence needing to support higher power.
We're considering 953 and 960 for the design.
Thanks!
Hello Speedah,
Normally we recommend a maximum Current over the PoC of 300 mA at 8V, but If you increase the Voltage to, say 24 Volt, then yes this is possible.
Thanks Hamzah! so this would put us at 7.2W. I see in this post that we may have higher current solution? Considering customer Vin is 12 or 24V, what would be the max power? I ask so that customer understand their limits for heater implementation.
I will double check with Sally and ask here to send you the contact details if you provide here with your email address.