Part Number: DP83848C
Other Parts Discussed in Thread: DP83848I
Hello,
I have designed the custom Ethernet board as like:
1) host computer : MPC860 / NXP
2) Ethernet PHY : DP83848C
- MAC Interface Mode : 10Mb SNI Mode
In Link-off condition, ping from MPC860 to other PC is OK,
but after Link-off and Link-on again,then MPC860 does not send TX signal normally.
To analysis the fault condition, I measured TX_CLK signal in DP83848C.
In normal condition, link-up, TX_CLK is 10MHz.
After that when link is changed into Link-off, TX_CLK is changed to 25MHz.
So TX_CLK, 25MHz, is asserted into MPC 860 that is set into speed 10Mbps.
Is it correct operation in SNI Mode of DP83848C ?