Part Number: HD3SS6126
Hi Please see the below configuration that I wish to use the USB passive switch.I wish to connect two USB port of a host PC to two inputs of the first HD3SS6126 and another two USB port of same host PC to the inputs of second HD3SS6126 .The common outputs of the two USB switches is conncted to the two inputs of third HD3SS6126.The output common terminal is connected to a USB flash drive.
Is the configuration works and if you could please let me know if any decrease in data transfer rate will occur.
Another Query
1.
What is the default impedance state (High/Low ) of the out put pins of HD3SS6126 .It is required to know the state to ensure the attached interconnection sequence(see the second image).