This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Strap resistors

Part Number: DS90UB954-Q1

Hi team,

We will use 954 that I2C address is 0x60(8 bit) or 0x7A(8 bit).

In this case, either the pull-up resistor or pull-down resistor is open.

The suggested resistor is 10kΩ and its tolerance is 1%, but in this case neither resistance nor tolerance is affected.

If Vidx satisfies the voltage range, 0Ω, short or any other resistance is acceptable.

Is it correct?

Is it still required 1% tolerance?

Best regards,

Tomoaki Yoshida