Part Number: DS90UB941AS-Q1
In the application notes document of DS90UB941AS-Q1, it is mentioned that in case of asymmetric splitting, resultant image will be produced at the half of the frequency of the superframe image. Is it meant to be that if we are producing superframe at 60Hz, DS90 will produced images for downstream display at 30Hz? If answer is yes how can 60Hz can be achieved for both displays?