Part Number: DP83867IR
Hello,
We are bringing up a custom board with a DP83867IR connected to a ZYNQ FPGA and are having packet loss issues. The problem exists
regardless of speed i.e. 10MB/100MB or1000MB. At 1000MB small packets under 32 bytes pass a ping test without issue, but larger packet sizes fail. We believe
we have configured the DP83867 correctly for loopback but we are not sure what IP address we should ping. We allow the device to auto negotiate,
so our assumption is that we will use the IP address configured during auto negotiation, is this correct? Can some one explain how the far end loop
works. We read the section in the troubleshooting guide, but it would seem like a ping to loopbacked phy would not have an IP address.
Thanks,
Ken