This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822H: LED_0/1 pins strap configuration

Genius 17995 points

Part Number: DP83822H

Hello,

I have one question for LED0 and 1 pins strap configuration.

There are two strap cases for LED0 and LED1 pins in Figure 31 of DP83822 datasheet (page 50).
Then I want to confirm right strap configuration for the below case.

  

In this case, I think Pull-down with1.96Kohm to 2.49Kohm on LED0 and 1 should work. Is it correct?

 

Regards,
Oba