Part Number: DP83849IF
Hi,
I am using DP83849if chip as RJ45(PORTA) to Fiber(PORTB) media converter and Maxim's MAX3799( laser driver and limiting amplifier) for the fiber optics conversion. MAX3799 has differential CML input and output.
From the other thread, I understood that DP83849if has differential CML inputs and outputs for the fiber operation.
Now the question is : 1. Should I follow the circuit for converting CML to PECL as shown in the schematic of the dp83849if evaluation kit ? or Should I connect the TD+- and RD+- pins without this?
2. Does signal detect input have to be connected for fiber optic operation? Any recommendation for connecting the LOS signal from MAX3799 to dp83849if?
Thanks.