Part Number: DS90UB926Q-Q1
Hello,
I have the following question below for Texas Instruments PN DS90UB926QSQX/NOPB. Can you help me find an answer?
There are two status output pins on the DS90UB926QSQX/NOPB deserializer IC that are stated in the specification as shown in the screen-shot below. I have a verification test to monitor each output in an overnight run by using an oscilloscope to probe each signal and trigger on the falling-edge. If the scope triggers, this would indicate an error and test failure. However, before I run this test I was hoping you could do a sanity check for me. I read the specification and my interpretation is that these outputs are only active during BIST mode. However, the definition doesn’t state that in the Status Pin Function section of the datasheet (pg7) from the specification so I am confused. I am wondering if you can confirm if the STATUS pins PASS and LOCK are active during normal running mode, or just in BIST mode?
Thanks,
Adam