Part Number: TS3USB221
Other Parts Discussed in Thread: TS5USBC41, TS5USBC402
Can you recommend a multiplexer that is suitable for USB Full Speed (12Mbps)? I am looking for:
- VDD = 5V
- 1:2 or 2:1 SPDT configuration
- Select pin
- Enable pin
Most USB multiplexers seem tailored to USB High Speed or USB Super Speed (TS3USB221 is a good example), with VDD limited to 3.6V. Given the slow data rates of USB Full Speed, I assume there is a suitable analog mux that is proven in this application.