Part Number: TMDS171
Hi
we have experienced a problem with the TMDS171.
We are using a video source which can be either with a 110MHz Pixel Clock or 140MHz Pixel Clock.
The TMDS171 on the display side is configured in "Automatic redriver to retimer mode".
In production we have found that even if on many units the display is working correctly, on some unit the display visualize a black image or an intermittent image/black image.
Analyzing the problem, the root cause was the TMDS171.
Changing the configuration of the TMDS171 to "retimer mode", solve the problem.
In your datasheet it is described that "The retimer is automatically activated at pixel clock above approximately 100 MHz" and that "At pixel clock below about 100 MHz, the TMDS171 automatically bypasses the internal retimer, and operates as a redriver." so, why in our case with a 110MHz or 140MHz pixel clock the device is not working in retimer mode??
Please clarify if we have not understood the modes of operation.
If we plan to use always the "retimer mode", what happens if the video source has a Pixel Clock that is <100MHz? Is it a valid operation mode or should we expect problems?
Thanks
Best Regards
Stefano