Part Number: DS90UB954-Q1
Hi TI team
About LINK_ERR _THRES, which default value is 0x3.
My customer want to change it to the max value (0xF).
But they concern about any other worse effects.
Could help to confirm whether the following items worsen or not, if changing LINK_ERR _THRES value from 3 to 15.
1. Cannot connect for a long time
2. Even if connected, video transmission is not possible for a long time
3. It takes time to detect a resurgence of contact
4. The video freezes or the image breaks between the counts of bigger than 3 and less than 15.