Part Number: DS25BR440
Other Parts Discussed in Thread: DS10BR150, DS15BR400
Hi
I have 2 questions about DS25BR440
1. This device can replace 4 of DS10BR150TSD.
2. Below schematic diagram is right for this device
BR
Hennessy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
1. The DS25BR440 may be used instead of four DS10BR150 devices. However, a quad version of the DS10BR150 is DS15BR400.
2. The schematic looks OK. I would add 0.1uF decoupling capacitor on each VDD pin.
3. The max IDD is 190 mA (PE=EQ=Off). The typical IDD is 162mA with PE=Off. Based on Figure 17 of the datasheet, the typical IDD with PE=On is ~195 mA. The estimated max IDD would be 20% higher. The EQ does not have an effect on IDD.
Regards,
Davor