Part Number: TCA9548A
Hi,
We got some question from the customer and there are some abnormal phenomenon. Can I ask some question ?
The situation,
1. The rise time of SC6 is almost 2.5us. (The input SCL is normal and also the fall time of SC6 is normal. The "normal" means these time are around a few 100ns.)
2. The other SCx signal has same phenomenon as SC6 as well.
(The customer condition is SCLK is 50kHz.)
(Question)
#1 I think the slow rise time such as above value is abnormal. Because it does not meet the I2C standards.
Standards , Rise time ; <1000ns (max) at 100kHz.
Is my understanding correct?
#2 We already had changed the pull up resistor but the phenomenon did not changed. (10k -> 2.2kohm)
Is there any other points to check ?
Best Regards,
Koji Hamamoto