Part Number: DP83867E
Other Parts Discussed in Thread: 66AK2H14, DP83867CS
8
Hello, I am using the DP8367 PHY to interface with the 66AK2H14 processor. I have wired the PHY to the ARM+DSP processor through the SGMII interface. I have not programmed the DSP/ARM with any boot code. When I plug in an ethernet cable to the RJ45 connector I don't see any LEDs toggling on LED_0 (LINK established) or LED_1 (1000BASE-T) link is established. I am connecting my board to a laptop so I thought I would see some leds flickering. When I plug the ethernet cable into the 66AK2H14 EVM it's leds flicker. Should I expect some flickering? LED_2 is always high.
Some say I won't see any action until the port on the ARM+DSP processor is configured but I'm not an expert in that area and we are working to configure/initialize the port now.
I have probed the CLK_OUT pin and I do see the 25Mhz Reference clock. I have also probed all the boot strap pins.
I just thought by simply plugging in an ethernet cable that is connected to a laptop that I would see seem of the LED toggling or stay on.
Here is my schematic
If anyone can help me please send me your comments.
Thank you,
Joe