Part Number: DP83867IR
Hi Team,
My customer is evaluating the DP83867IRRGZ (RGMII), and they have some questions as below.
Q1: 100-Mbps Transmit Timing under RGMII MAC Interface Mode:
Which TX_CLK edge, rising edge or falling edge, is the TDX[3:0] data latched on?
If the Bit-1 of RGMII Control Register (RGMIICTL, 0x0032) is set "1", RGMII transmit clock is shifted, under 100-Mbps mode, how much RGMII Transmit Clock Delay is allowable?
Q2: 10-Mbps Transmit Timing under RGMII MAC Interface Mode:
Which TX_CLK edge, rising edge or falling edge, is the TXD[3:0] data latched on?
If the Bit-1 of RGMII Control Register (RGMIICTL, 0x0032) is set "1", RGMII transmit clock is shifted, under 10-Mbps mode, how much RGMII Transmit Clock Delay is allowable?
Thank you.
Best Regards,
Koshi Ninomiya