This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4E1U06: Design review

Part Number: TPD4E1U06


Hi,

Please let me know wether reverese polarity signals connected to pins.

i.e wether negative signals connected to pin 1 and 3 and positive signals connected to pin 6 and 4.

  • Hi Shifali

    The TPD4E1U06 is a unidirectional device with a working voltage of 5.5V referenced to ground. If I understand correctly you are asking if you can connect a negative signal to pin 1 and 3. This is not recommended since it would only  tolerate a negative voltage of around -0.5V in normal operation.

    For devices hat would tolerate a negative signal you may want to consider the TPD4E1B06

    Thanks,

    Obi