Part Number: SN65DPHY440SS
Hello,
I'd like to confirm if SN65DPHY440SS support polarity inversion, the datasheet describes that it doesn't support polarity inversion, and the below post is the same with datasheet, but as my opinion, it would be fine only if the same polarity maintained between the source and sink, because the differential signals between P and N are opposite, which one is used P or N should be no problem and I don't understand why SN65DPHY440SS couldn't.
Thank you very much for your reply.
Best regards
Kailyn