Part Number: TPS65988
Hi, everyone,
In our design,
- Both of 2 Type-C ports are DRP.
- Only one 1 ports can supply source power with our products.
(We cannot receive power from 2 ports simultaneously.)
Now we assume that
in one side Type-C port, PD adaptor is attached and supplies VBUS=5V,
and the other side Type-C port, PD adaptor is attached and supplies VBUS=20V.
If both of these 2 Sink path FET are ON, these VBUS lines are shorten,
which results in overcurrent.
Does any protection function by TPS65988 work if these 2 Sink path FETs are ON by mistaken?
Or do we have to add external protection circuit around TPS65988?
(ex: VBUS reverse protection circuit.)
Best Regards,