Part Number: TPS65982
Can i use TPS65982 USB2.0 lines to program MCU (MSP430) that writes TPS65982 firmware to flash memory afterwards?
The device that im working on is an alternative mode , for displayport. I need the TPS65982 to power MCU and allow it to use its USB 2.0 lines , to program the MCU. Then i want to use the MCU to write the TPS65982 displayport firmware to flash memory , that is shared with the MCU.
The question is- "Will TPS65982 power the MCU and allow it to use the USB2.0 lines to program it , if the flash memory is empty at the begining? "