This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCA9306: PCA9306 Level shifter

Part Number: PCA9306

Hello team,

my customer wants to use this PCA9306 Level shifter.

I want to understand how many components I can connect to each side? Is there a limit?

I see on TI’s ref. designs that there are several components connected, but I just want to make sure:

Could you please advise back, thanks in advance.

Best Regards,

Shai

  • Hi Shai,

    The device itself doesn't impose a specific limitation, but the total load capacitance (including components on both sides) should not exceed 400 pF per I2C standard limits. If you need to support higher capacitance, you might consider a buffered level translator instead.

    Regards,

    Max