Part Number: DS80PCI800
Dear,
For DS80PCI800, if the rate is setting as float(Auto rate select of Gen1/2 and Gen2 with De-emphasis), customer want to know how to select the correct Level in table 3 in datasheet for Gen3 application?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS80PCI800
Dear,
For DS80PCI800, if the rate is setting as float(Auto rate select of Gen1/2 and Gen2 with De-emphasis), customer want to know how to select the correct Level in table 3 in datasheet for Gen3 application?
Thanks.
Hi,
The correct setting for PCIe Gen3 applications is "Float".
FLOAT = AUTO Rate Select of Gen1/2 and Gen3 with de-emphasis
Regards,
Lee
Hi Lee,
Could you please advice how to select the proper level in table3 for Gen3 application?
Thanks.
Hi,
The RATE pin should be set to "Float".
Table 3. Sets the output amplitude and de-emphasis. In most PCIe applications a setting of "Level 4" in Table 3 will work well.
This setting gives enough amplitude for the PCI800 to be transparent to most incoming Tx FIR waveform information.
Regards,
Lee
Hi,
Additional information: Since system PCIe Tx's will already add Tx equalization to the signal, the redriver usually does not need to add any additional Tx equalization. It will only use its input CTLE (Rx equalization) to help restore and redrive the original signal.
Regards,
Lee