Part Number: TLK2501
Dear Team,
My customer is working with the TLK2501 for the past 10 years.
In recent design they have an issue regarding PLL lock signal.
They are connecting pin # 41 – RX_CLK to a MMCM input of ARTIX7 FPGA from XILINX.
From time to time, when we power the system at minus 30 degC , the MMCM reports that the PLL is not locked, and after a few seconds it is locked again.
We suspect that this is a jitter issue. The maximum allowed jitter at the FPGA MMCM input is 80 psec.
I don’t see at the TLK2501 datasheet the maximum jitter on the TLK2501 RX_CLK output (including all temperature scale)
Can you advise ?
Regards,
Nir