Part Number: DP83822IF
Hi team,
About the MAC interface mode of DP83822, the datasheet says the device can work at RMII master or slave mode. However, it seems we can only select enable or disable RMII mode through pin strap. The datasheet does not say how to select master or slave mode.
Also, as my understanding, the device can only works in RMII master mode if the reference clock is generated from 25MHz crystal, and It can work in master or slave mode if it is clocked by 50MHz oscilator. correct?
Thank you,
John