Part Number: LMH1297
Other Parts Discussed in Thread: , SIGCONARCHITECT
Hi, team:
We develop a 12G-UHD converter product using LMH1297. We use PHABRIX QX12G to generate 12G color bar signal to our board. The cable is belden 4694R+Amphenol 31-70548-12G plug. BNC socket on the PCB is samtec BNC7T. Lock status from LMH1297 is locked when cable length is 1m , but the HEO/VEO read from LMH1297 is 0.59UI/178mV. This value is very low. When we use 30m cable, the signal is unlock frequently.
Lmh1297 datasheet said it can suport up to 65m , how can I increase the HEO/VEO by setting register? Our customer need to run at 30m.
I think our PCB layout has no problem, we use SAMTEC's recommended design, and we have passed high speed SI simulation and final PCB TDR test.
Thanks a lot.