Part Number: TPS65987EVM
I have just purchased the TPS65987EVM with FTDI chip and cannot get the unit to flash using the Application Customization Tool.
The error I keep receiving is:
Exception Encountered during SPI Flash to Device:No FTDI I2C channels (I2C_GetNumChannels) detected, exiting....
<type 'exceptions.Exception'>
In the Show Details I get:
Traceback (most recent call last):
File "dialogWindow.pyc", line 3393, in flash_device
File "hw_interface.pyc", line 187, in hw_open
Exception
Under the device manager I can see 4 USB Serial Com ports with no errors and the ports go away when I disconnect the usb cable so it appears the FTDI unit is connected.
I would appreciate any help I can get for this problem.