This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987EVM: Cannot get it to flash or communicate using the Application Customization Tool.

Part Number: TPS65987EVM


Hi,

My customer is having issues flashing the unit through the application customization tool. 

Below is the error:

 

Exception Encountered during SPI Flash to Device:No FTDI I2C channels (I2C_GetNumChannels) detected, exiting....

<type 'exceptions.Exception'>

In the Show Details I get:

Traceback (most recent call last):

File "dialogWindow.pyc", line 3393, in flash_device

File "hw_interface.pyc", line 187, in hw_open

Exception

Under the device manager I can see 4 USB Serial Com ports with no errors and the ports go away when I disconnect the usb cable so it appears the FTDI unit is connected. I am using Windows 7.

I appreciate the support.

Thanks,

Kevin