Part Number: DP83849IF
Hi,
I am using DP83849if chip as RJ45(PORTA) to Fiber(PORTB) media converter.
Information about my application:
Board A Board B
(RJ45+magnetic <--> DP83849if <--> FX_transceiver) <--> FO cable <--> (FX_transceiver <-->DP83849if <--> magnetic+RJ45).
I use ping test to check communication between Board A & B. But I do not receive an answer.
I have attached the registers value read by µC.
1. Could you please check and let me know if the configuration settings(porta and portb) for this setup are correct?
2. Which register can give me information about the received data from FX differential signals?
3. When RJ45 is not connected, I could see the default pattern of 125MHz signal generated by Dp83849if on the FX transmit differential signals. Is that correct or something wrong ?
Thanks and Regards,
Yash