Part Number: TCA9555
Our TCA9555PWR is consuming a mystery 2.1mA. We can remove it from the board and see the overall current drop by that much.
The datasheet indicates that in operating mode or when there are high inputs, the current is a few uA. When there are low inputs, the datasheet says ithe part would would consume ~0.6mA. Is this actually the case that a low input would cause the part to consume > 1mA?
We assumed when selecting the part that this part of the datasheet was a typo and that the part should consume only uA.