Part Number: SN75DP130
Hi Team,
Customer is using DP130 and customer has question on the reset pin level question.
Would you please recommend the proper solution for this?
- What is the reset low level? 0V~0.8V? then, 0.75V is low level or high level?
- What is the reset high level? 1.9~3.6? or 0.75V~3.6V?
- From the below table, please provide your comment for the reset right level.
BR,
SHH