Part Number: DP83869HM
* Config
- Configure the media converter using the DP83869HM device.
- The front end uses Giga-bit RJ45 Copper SFP module.(1000BASE-FX)
- Rear end uses RJ45 connector.(1000BASE-TX)
* Problem
- The network connection status of the front and back stages is confirmed by the computer, but when the ping test is performed, the result is displayed as a failure.
* Requirements
- Request for a design review and response to the attached schematic.
Thanks:)